Industry Online Support
Technical Forum
9/17/2013 4:10 PM | |
Posts: 5 Rating: (0) |
Sinumerik 802D SL works now with Sinamics S120. System shows following faults: 231897|Axis Z1 drive 2 DRIVE-CLiQ: No communication to component. Preliminary component number: 4. 231885|Axis Z1 drive 2 CU DRIVE-CLiQ: Cyclic data transfer error. 15 hex. 231851|Axis Z1 drive 2 CU DRIVE-CLiQ: Sign-of-life missing. a hex. 25201| Axis Z1 drive fault 700033|User alarm 34(this is an interlock, oil pump should be on before starting system, so it is not important) (F31897,F31885,F31851 - List Manual S120/S150) In the STARTER archive (160913_VERTLATHE.zip), one can see that component number 4 correspond to SERVO_03.SMI20_4 COMPONENTN° VERSION FW TIPO REFERENCE VERSION HW SERIAL NUMBER CU_I_003.Control_Unit_11 2406300 Control Unit 6FC5370-0AA00-0Axx A T-P30050000 SERVO_02.Motor_Module_2 2 2503221 CUA6SL3040-0PA00-0Axx DT-B12013939 SERVO_02.Motor_SMI_9 9 --Motor 1FK7083-xAF7x-xKxx B930 0996 02 005 SERVO_02.Encoder_8 8 --Encóder 1FK7xxx-xxxxx-xKxx T-B88262342 SERVO_02.SMI20_7 7 4402313 SMI20/DQI6SL3055-0AA00-5Mxx HT-B88262342 SERVO_03.Motor_Module_33 2503221 CUA 6SL3040-0PA00-0AxxD T-B72000989 SERVO_03.Motor_SMI_6 6 --Motor 1FK7063-xAF7x-xKxxB 826 8654 03 001 SERVO_03.Encoder_5 5 --Encóder 1FK7xxx-xxxxx-xKxx T-B72047873 SERVO_03.SMI20_4 44402313SMI20/DQI6SL3055-0AA00-5MxxH T-B72047873 As there are two SMI20/DQI in the topology, one for each motor module/encoder's axis (vertical lathe only has two axis), I exchange the cables (profinet cable), to see if the faults also change from axis Z1 to X1. That was the case! After I only change the cables, the problem change from axis. But I don't know if the cable or the device is faulty? And why would the device be faulty, the machine arrived in 2012, not long ago... I think the problem is hardware, because Sinumerik 802D SL has a buil-in function to: Load Sinamics Firmware, Load default parameters and Topology recognise. So Software is well configured, as it should come from factory. One should not change anything, in order to work...? I have tried different methods, I investigate about the faults, but I don't find to get anywhere. Still stuck with the same faults. Do you have any indication or recommendation? How could I be sure that the devices is faulty? AttachmentC:\Documents and Settings\z0033s5u\Desktop\160913_VERTLATHE.zip (218 Downloads) |
6/12/2017 4:49 PM | |
Posts: 6 Rating: (0) |
problem with smi20 so change same smi then check alarm will clear so trail purpose u can use same model no smi if alarm reset then problem is smi only . |
Follow us on