5/10/2018 9:45 AM | |
Posts: 2 Rating: (0) |
I own your Simens Sinamics v20 frequency converter of 0.75kW and I have a problem with the connection I can not set the inverter to control it with external potentiometer and external switch for start and end of motor rotation. My desire is to set the desired engine speed with the external potentiometer and then start the engine with an on / off switch. I have not been able to get together any of the settings I used. Please help in configuring and connecting the external wiring of the frequency converter Nice regards ------------------------------------------------------------------------------------------ |
Last edited by: Mirager44 at: 5/10/2018 9:45:53 AMLast edited by: Jen_Moderator at: 5/11/2018 10:01:38 AMNew subject after splitting |
|
5/10/2018 10:48 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello, Please download & refer SINAMICS V20 Inverter manual. Refer page no 6 for electrical wiring diagram & chepter 3.2 quick commissioning page no 12. HTH. |
Last edited by: Jen_Moderator at: 5/11/2018 10:05:01 AMOptimized link. |
|