6/21/2014 2:53 PM | |
Joined: 2/19/2013 Last visit: 5/23/2024 Posts: 184 Rating: (8) |
I have it connected in this way: |
6/22/2014 4:34 PM | |
Joined: 2/19/2013 Last visit: 5/23/2024 Posts: 184 Rating: (8) |
I get it. And now what do I have to do to get this output working? |
6/23/2014 9:50 PM | |
Posts: 5225 Rating: (1188) |
Hi Adrian, You have now.. B701 = 1 B702 = 12 --- right? By now you should have the manual from.. LINK Please go to page 156, and look for "ON reverse / OFF1". w |
8/9/2017 10:25 PM | |
Joined: 8/9/2016 Last visit: 6/1/2024 Posts: 70 Rating: (0) |
Definitely. Unfortunately i come across this problem 3 years later. |
8/29/2017 11:24 AM | |
Joined: 3/31/2015 Last visit: 1/26/2024 Posts: 175 Rating: (16) |
Because there is no minimum voltage. It'll pass anything up to max values. |
9/21/2017 5:11 PM | |
Joined: 9/1/2015 Last visit: 4/11/2024 Posts: 13 Rating: (1) |
Official Siemens answer is 3-35V DC. I've tested it with 12V DC and it works fine!! Hope it helps! Regards! Chucky! |
11/13/2017 7:12 AM | |
Posts: 1 Rating: (0) |
Why do I attach 24V to DO1, DO2 to the relay and then to 0V when the transistor also leads? What if I want the transistor to stop? |
Follow us on