5/2/2023 8:07 AM | |
Joined: 10/18/2016 Last visit: 11/27/2024 Posts: 22 Rating: (3) |
Hi Kunetoh, i can't say anything about IOT2050, I only know the CM PtP but if you can already read and write values then it should work. However I guess you have a problem with the format of your Modbus request if you receive an Modbus error. What exactly are you trying to do and which error do you receive? Also take a look into V20 manual to see all Modbus registers and supported function codes. Best regards, DaMo |
5/9/2023 5:53 AM | |
Joined: 12/16/2021 Last visit: 8/22/2023 Posts: 126 Rating: (2) |
Hi Kunetoh, Solution for 1st IOT2050 connection system through industrial edge, cloud system and IOT Solution for 2nd 1. Download latest manual of v20 from here Follow instruction for basic inverter seting for modbus communication as shown in manual. 2. Set parameter as mentioned step by step in manual
|
If The Information Helpful, Then Don't Forget Give (To thank ) and Rate It |
|
Follow us on