2/25/2022 2:40 PM | |
Joined: 10/24/2013 Last visit: 1/12/2025 Posts: 47 Rating: (0) |
i tried to do what you recommend but i didn't find telegram 750 and in tia 16 i can only add one telegram |
2/28/2022 9:25 AM | |
Joined: 4/28/2015 Last visit: 10/22/2024 Posts: 1278 Rating: (301) |
I just tried it out myself. In TIA there are 2 options how to integrate the V90PN: 1. via GSD file 2. via Hardware Support Package (HSP) No matter which way you choose - for both it is possible to add telegram 750. Please see my attached screenshots. I also made one of a simple PLC program to read out the telegram data. AttachmentScreenshots_TIA.zip (840 Downloads) |
Best regards, |
|
This contribution was helpful to2 thankful Users |
Follow us on