10/25/2022 7:02 AM | |
Joined: 5/19/2014 Last visit: 9/1/2024 Posts: 8 Rating: (1) |
Hi Baacus, I faced similar problem. I am using sina_pos (S7-1200+V90 via profinet). When V90 performs short fast shaking moves (3 times +-10mm in ~400ms) sometimes sina_pos ignores next fast ExecuteCmd. I solved this problem by repeating Execute command after 500ms to sina_pos when drive not moving is detected, but it delays my sequence time . Using AxisPosRef positive edge did not solve problem. I suppoused some dalays in network. Have somebody face this problem and have somebody solution for this ??? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/25/2022 08:54:59New subject after splitting |
|
Follow us on