1/5/2014 9:31 AM | |
Joined: 8/31/2010 Last visit: 2/8/2025 Posts: 1524 Rating:
|
Hello pratik7332, CP 1242-7 is a product. SINAUT is the brand. which product in SINAUT do you mean? Is it MD 720-3? If it is so, then CP 1242-7 is a module which gets connected in the backplane of S7-1200 system. Whereas MD 720-3 needs to be interfaced with PLC through RS232 interface. Application Example - CP 1242-7 - Wireless signaling and switching via SMS with S7-1200 Controllers (Set 32) MD 720-3 - Wireless Signaling and Switching via SMS with serial CPs/CMs and the MD720-3 GPRS/GSM Modem |
Like it? Rate it! |
|
1/7/2014 8:25 AM | |
Joined: 11/26/2009 Last visit: 3/16/2025 Posts: 223 Rating:
|
hi, I got it, thnx for the info i want to interface MD720-3 with S7200 . which MLFB number to order ?
|
1/7/2014 8:43 AM | |
Joined: 8/31/2010 Last visit: 2/8/2025 Posts: 1524 Rating:
|
Hello pratik7332, S7-200 is declared as a Phased-Out system. You may go ahead with S7-1200 + CP 1242-7 soluation, which is feasible both technically and commercially. You may contact your nearest sales office. Contacts Worldwide |
Like it? Rate it! |
|
Follow us on