9/5/2014 2:08 PM | |
Posts: 3 Rating:
|
Dear Experts, I would like ask you about an issue about SINAUT ST7 -Redundant Connection. My application is Redundant IP Connection (IE and MSC Page 25 Of the attachment) Could you please help me with the bellow?
As I can see In the diagram I use one module for the Wireless Ethernet connection and GPRS(MSC) and the other module for the Control Center(ST7 cc) My Question is in Which port of the second module I have to connect to the Control Center?Also I would like to clarify if I need to set the module (Subnet and IP) same as the Control Center.
May I use an other Object for that purpose? I want the Control Center sending to PLC INT and DINT Variables.
AttachmentSINAUT ST7 - Redundant Connections.pdf (99 Downloads) |
Follow us on