7/16/2016 7:12 AM | |
Posts: 92 Rating:
|
Hi there im work on a Sinumerik 810T GA2 and PCIN on Windows XP in PC Im also online and my cpu type is :150U my Backups file all is as a ".txt" f.e : PCP.txt PCA.txt TA1.txt and ... Bout rate in PCIN,COM por setting,Sinumerik810 :300 Or 11000010 5010/5012 :00000000 5011/5013 : 11000010 5016 : 00101000 I set my cable like this,with sheald and earth protection: 9 PIN 25 PIN 1--------1 sheeld 2--------2 3--------3 4--------6 5--------7 6--------20 7--------5 8--------4 same as the pcin comment. To be sure as The whole memory is erased , i remove my battery after that start to inittial. I can Download %TEA1 and %TEA2 as well as,But when i want to Download %PCP ,after 1800 Byte,DIO will disappear and transfer will be stopped. Also i can Download other Machins %PCP to this system control , its work as well as! But system controls own %PCP ,Not. I've been Try Many things with diferent cable's,but same result. I'm suspicious to this : At the friest,I Do step by step any thing in reload pdf file,but after second reset(after Download TEA1 and TEA2 ) I need to press "END stup PW" and Press diagnosis,then Eyeball, pasword-->enter But when I press Inittial clear mode ,its show : NO Key-Operated Switch Here is photo so i have to hold Eyeball agein and go to Initiall clear mode
thanks a lot for your attention Best regards ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 7/18/2016 12:39:18 PMNew subject after splitting Last edited by: Sky Diver840 at: 8/2/2016 8:58:45 AM |
|
7/28/2016 11:40 AM | |
Posts: 92 Rating:
|
I Attached Files And Picture of "NC ALARM " And transfering %PCP. And Here is Alarms Too: [ NC ALM : 3 ORD 1 Plc stop Alarm message from NC 3 ORD 1 Plc stop 2153 ORD 2 control loop Spindle - HW ] [ PLC ALM : 3 ORD 1 PLC STOP Alarm message from plc 6127 alarm byte messing ] [ PLC MESSAGE :
PLC MESSAGE ] AttachmentPic Of ALA & PCP TRNSFR.zip (708 Downloads) |
Follow us on