Industry Online Support
Technical Forum
8/10/2012 7:34 PM | |
Posts: 10 Rating: (0) |
I have some alarms related to hidraulic pressure, but all can be reset from that panel which is blinking ....any suggestion? |
8/12/2012 3:36 PM | |
Posts: 10 Rating: (0) |
I've measured it when I made the picture, the voltage was 3.11 V on the Extension board, and 3.10 V on the MCI, thanks again for the help Kind regards, Marius |
8/12/2012 4:26 PM | |
Posts: 10 Rating: (0) |
if I remember well both batteries are 3V, that is why ....I skipped this possibility ... |
Follow us on