3/6/2019 7:34 AM | |
Joined: 9/28/2007 Last visit: 12/28/2024 Posts: 235 Rating:
|
Dear Experts I have sinumerik 840D Control. When i input command M2=19 and execute it moves spindle and stop at angle of 45 degree but i want to stop it at 90 degree. is there any possibility to change the spindle degree according to my requirements. i also want to know the complete description related to spindle orientation parameter and configuration. how sinumerik works when i enter M2=19 command. i also used SPOS=90( but no response from machine).. i want to understand sinumerik and plc programming for spindle orientation and how can i change it to my own requirements.. |
Muhammad Munir |
|
3/6/2019 1:19 PM | |
Joined: 10/27/2009 Last visit: 3/15/2024 Posts: 455 Rating:
|
Your command "M2=19" is a spindle orientation command for spindle #2. The spindle position for orientation by M19 is to be define in a SettingParameter
By programming via "SPOS" You can define the orientation position directly by definition of the spindle number in square brackets:
Your test via "SPOS" (without spindle index in square brackets) is always related to the MasterSpindle. |
hope that helps |
|
This contribution was helpful to
2 thankful Users |
3/7/2019 5:29 AM | |
Joined: 10/17/2007 Last visit: 3/21/2025 Posts: 4249 Rating:
|
Do you read answer from CNC600, that is the simplest solution just remind you --that easy to access --go to "Parameter"-->Setting Data--> Spindle-->xxx
|
If you like my comments please |
|
This contribution was helpful to
1 thankful Users |
3/7/2019 7:56 AM | |
Joined: 9/28/2007 Last visit: 12/28/2024 Posts: 235 Rating:
|
Dear Sir I read the answer and i did as you said. i go to parameter ---->setting data but there is no parameter number SD43240?? There is only 6 to 7 parameter visible. how can i see that parameter? i tried another SETUP--------> Machine Data------> General MD(10000--->19800) Channel MD(20000---29000) Axis MD(30100---38010) Driver MD(1000---4725) Display MD(9000---9999) Dear Sir I find it in parameter---> Misc-----> Axis specific Data-->43240 value of 43240=0 i changed it to different angle but spindle always stop at same angle(22 degree), there is no change in spindle orientation with M19 command.. I used SPOS[2]= 90 then spindle change its angle at 90 degree. i can change spindle angle with SPOS[2]= 90 but M19 is not working like i want.. when i enter M2=19 spindle always orient at same angle.. what is the problem, why spindle stop at same angle.. Dear Sir today i tried again and now this time i successfull.. i am little bit wrong. paramter----> setting data----> Misc-----> Axis specfic data----> then upper left corner , ichanged Axis to SP2 then edit 43240= 136 and now M2=19 works and spindle stop at 136 degree... |
Last edited by: mmkhan at: 3/8/2019 5:18:48 AMLast edited by: mmkhan at: 3/8/2019 2:40:05 PMMuhammad Munir |
|
3/11/2019 5:50 AM | |
Joined: 9/28/2007 Last visit: 12/28/2024 Posts: 235 Rating:
|
Dear Experts Problem solved. |
Muhammad Munir |
|
We are working on a new user interface with better overview and more relevance.
Follow us on