Industry Online Support
Technical Forum
1/23/2011 1:31 AM | |
Posts: 3 Rating:
|
Hi guys i've been having a problem with my Siemens Sinumerik PCU 50, it just does not want to boot up into the system. It was working fine then all of a sudden the screen showed a few red lines then it shut off. I went to boot it up and it would not go past the the bios screen. I can get into the bios by pressing F2. It simply will not load/boot up into the operating system. I did notice that on the back of the control box towards the bottom right there are 4 LED's that light up. When i switch the power on the first led lights up Red for a split sec thens goes away, the second led does nothing, the third one lights up green and stays solid the whole time and the fourth one flashes orange for the entire time. To me it seems like they could be diagnostic LED's, but i cant seem to find any information about those LED's. BTW what is this "extended RAM"? (look at pic below) I will provide links so you can see the specs and a video of what is happening. VIDOE LINK: http://www.youtube.com/watch?v=MkuwBceEmkY Thank you guys for the help.
AttachmentIMAG0123.zip (166 Downloads) |
Last edited by: O_Moderator at: 1/23/2011 11:15 AMpictures transferred to attachment Last edited by: Luca451 at: 1/23/2011 2:23 AMLast edited by: Luca451 at: 1/23/2011 2:22 AMLast edited by: Luca451 at: 1/23/2011 1:54 AMLast edited by: Luca451 at: 1/23/2011 1:43 AMLast edited by: Luca451 at: 1/23/2011 1:40 AMLast edited by: Luca451 at: 1/23/2011 1:39 AMLast edited by: Luca451 at: 1/23/2011 1:38 AM |
|
1/25/2011 8:16 AM | |
Posts: 3 Rating:
|
In the video the orange light is flashing, but for some reason when I took the video the "flashing" would not show up. |
1/25/2011 8:23 AM | |
Posts: 3 Rating:
|
since my orange light is flashing what would that mean? |
1/25/2011 12:05 PM | |
Joined: 1/19/2008 Last visit: 11/29/2023 Posts: 976 Rating:
|
Hi, It means as Ekalavya says in his post that your machine control panel is working very well. Pee |
4/18/2019 8:50 PM | |
Joined: 11/26/2016 Last visit: 10/8/2023 Posts: 138 Rating:
|
I now face the same problem, and I want the solution. |
Nothing IS IMPOSSIBLE. |
|
Follow us on