Industry Online Support
Technical Forum
1/20/2013 10:32 AM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating: (71) |
Hi I have configured Siprotec 7SJ80 in hardware configuration. Have downloaded the required configuration through DIGSI to relay and device status shows that DATA_EXCH. Also when I see hardware configuration online it says that module is available and healthy. But in PCS7 driver block of 7SJ80 shows the error code "16#2021" which according to help file means "Hardware Config.: Slave or slot does not exist". I have configured the slave address, DP Master system number (Subnet ID) and type of Mapping being used in driver block,but still this error remains. Also when I unplug the relay from profibus error code remains exactly same. What is wrong? Any input on this regard would be of great help. Regards Manmeet Attachmentsiprotec.zip (117 Downloads) |
This contribution was helpful to1 thankful Users |