8/17/2007 12:50 PM | |
Posts: 151 Rating: (8) |
Hi Djordje, you can try to connect the sensor without smartplug wires. Refer to page 3-15 of the manual for the wiring, leave the smartplug wires disconnected. On page 4-3, you can read how to configure the flowmeter when a sensor without smartplug is connected. This is possible, because there are sensors without smartplug which are compatible with the intermag 2 (for example the 711/S). As you can see, you need some additional information of the sensor. Hereis the link to the manual. http://support.automation.siemens.com/WW/view/en/7915331 Good luck, SonicRanger. |