3/25/2021 7:41 AM | |
Posts: 1 Rating: (0) |
Hello all, i have having problem in Sitrans probe LU level transmitter. It is showing wrong level while feeding in the tank. i checked the location of the transmitter but it is ok i.e LT is far away from the feeding line. When the feeding stops then the level is stable. Kindly help ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/25/2021 10:22:21New subject after splitting |
|
Follow us on