11/27/2012 1:40 PM | |
Joined: 8/16/2010 Last visit: 4/24/2024 Posts: 636 Rating: (12) |
Hi all, Is there modul like SIWAREX for s7-1200 CPU? Which alternative modul to use? Best regards, Miloš |
11/27/2012 2:15 PM | |
Joined: 8/31/2010 Last visit: 4/29/2024 Posts: 1509 Rating: (222) |
SIWAREX WP231 |
Like it? Rate it! |
|
This contribution was helpful to2 thankful Users |
11/27/2012 2:33 PM | |
Joined: 8/16/2010 Last visit: 4/24/2024 Posts: 636 Rating: (12) |
Nice. Do I need some HW catalog to update TIA or some additional software for WP231 module? |
11/28/2012 2:37 PM | |
Joined: 8/16/2010 Last visit: 4/24/2024 Posts: 636 Rating: (12) |
Thanks, Ganes10. Is that some short period or middle of the next year or... |
12/10/2012 12:58 PM | |
Posts: 206 Rating: (22) |
Hello, the WP231 is now released. You can find information's at www.siwarex.com . You need a configuration package for the WP231 the order no. is 7MH4960-2AK01. Regards ABenno |
12/10/2012 1:50 PM | |
Joined: 8/16/2010 Last visit: 4/24/2024 Posts: 636 Rating: (12) |
Ok, thanks for information. But where we can download hw catalog for that module? I can't find anywhere. |
12/10/2012 2:15 PM | |
Joined: 8/31/2010 Last visit: 4/29/2024 Posts: 1509 Rating: (222) |
Hello Milosh, You have to wait till it is pubished here - STEP 7 (TIA Portal) V11 Support Packages for the hardware catalog in the TIA Portal |
Like it? Rate it! |
|
12/11/2012 1:15 PM | |
Joined: 8/31/2010 Last visit: 4/29/2024 Posts: 1509 Rating: (222) |
Hello ABenno, Find the sample program using STEP 7 and WinCC v11 - TIA-Portal program "Ready for use" for SIWAREX WP231 Only the HSP is yet to be released and the supported version along with the SIWAREX WP231 library. When I tried opening with v11 SP2 Upd 4, the WP231 device is shown as not available and it's properties are not visible. |
Like it? Rate it! |
|
12/12/2012 1:43 PM | |
Joined: 8/31/2010 Last visit: 4/29/2024 Posts: 1509 Rating: (222) |
SIWAREX WP231 electronic weighing system - for your reference |
Like it? Rate it! |
|
2/20/2013 11:22 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Most probably with the next released of TIA12. Who knows! Best regards, Hristo Mihalev
|
Follow us on