1/16/2018 12:07 PM | |
Posts: 2 Rating: (0) |
Hi! I have also the same situation with 2 modules Siwarex 7MH4950-1AA001. At first of them I have SF led, 24V lighted and the 6-th LED bilnking; this one don't weigh. But the second module, have all 6 LED's lighted and keep the CPU in STOP mode. Which is the role of the 6th led Can I do something with them? Many thanks in advance! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/17/2018 9:24:13 AMNew subject after splitting |
|
Follow us on