Industry Online Support
Technical Forum
1/1/2009 8:35 PM | |
Joined: 9/27/2006 Last visit: 12/10/2024 Posts: 12302 Rating: (2692)
|
Hello Alin; To provide both the 24 V and 5 V required to use the Siwarex U as a standalone unit, Siemens strongly suggests you set it up with a ET 200M interface (that would imply IM 153-2 +PS +rail and bus connector); see the following FAQ discussing different Siwarexmodules as standalone units: http://support.automation.siemens.com/WW/view/en/10183487 Hope this helps, Daniel Chartier |
Follow us on