5/27/2014 11:34 AM | |
Posts: 63 Rating: (4) |
porgrammed FC pic
AttachmentF:\siwarex\FC80 prgrammed for reading siwarex u weighing and fault status.jpg (288 Downloads) |
5/27/2014 11:35 AM | |
Posts: 63 Rating: (4) |
UDT content pic from Siwarex manual. |
5/28/2014 6:05 PM | |
Joined: 1/4/2007 Last visit: 12/10/2024 Posts: 1158 Rating: (175)
|
Hello MHasan, I recommend you to use the S7 example programm “SIWAREX_U_GETTING_STARTED_S7.zip” which you can find on the internet: http://support.automation.siemens.com/WW/view/en/28391777 At the FB45 you can see at the parameter “GROSS1” the current weight value of channel 1 and at the parameter “GROSS2” the current weight value of channel 2. Best regards Siwarexi |
5/29/2014 6:49 AM | |
Posts: 63 Rating: (4) |
Hello Siwarexi I have the S7 example programm “SIWAREX_U_GETTING_STARTED_S7.zip”.But i dont want to use this program because if i can set parametesr of siwarex module with SIWATOOL 2 U software then i only need to extract values of gross weight and fault as mentioned above in my post. With this program it looks to me i have to consider many other aspects as well. Thanks |
Last edited by: MHasan at: 5/29/2014 6:51 AM |
|
1/7/2015 11:02 AM | |
Joined: 9/16/2013 Last visit: 1/27/2022 Posts: 17 Rating: (1) |
Well I got it all. Thanks a lot for your concern. Best regards,
|
Follow us on