Industry Online Support
Technical Forum
8/2/2013 10:09 AM | |
Posts: 206 Rating: (22) |
Hello Norikafu, you can use a much WP231 modules as the CPU allows as modules in general. You also ahe to watch the memory and the I/O space that the CPU provides. The WP231 needs 16byte of in- and output space. As memory 3750bytes for the function block is needed and additional 990bytes for each WP231 data blocks. If you are using Modbus for communication you have to refer to the Modbus "Master" restrictions, on the WP231 side thereare nor restrictions, you just need to give eachr WP231 a unique address. See also the manual chapter 5. The manual you download here: http://support.automation.siemens.com/WW/view/en/64722267/133300 Regards ABenno |
Last edited by: ABenno at: 8/2/2013 10:20 AM |
|
Follow us on