2/27/2018 4:13 PM | |
Joined: 1/17/2013 Last visit: 7/25/2023 Posts: 7 Rating:
|
[snip] I have in total 12 WP321 modules. So basicaly 3 scales and each uses 4 WP321 modules. In any case you can maybe help me with programming of the cells . I have 4 cells on 1 platform to measure weight of the tundish. Problem now is that i know total load on 4 cells but it is impossible to calibrate each of the cells separately. Tried to play with auto calibration and with number of support points but with no success. Have checked load cell parameters as maximum load and mv/V settings. I attached picture of 1 part of platform, other part with other 2 cells is identical. so they can just put cumulative load on all of 4 cells. Problem is that i can't know how load is divided between this 4 cells. Kind greetings ------------------------------------------------------------------------------------------ |
Last edited by: It_Is_I at: 2/27/2018 4:14:59 PMLast edited by: It_Is_I at: 2/27/2018 4:16:27 PMLast edited by: Jen_Moderator at: 2/28/2018 9:13:37 AMNew subject after splitting. Division of questions into separate topics. |
|
Follow us on