Industry Online Support
Technical Forum
1/22/2013 8:54 PM | |
Joined: 2/22/2006 Last visit: 1/23/2023 Posts: 7 Rating:
|
Issue: After 1-2 weeks, two of four OS Clients need to be restarted, because the response time of the clients gets very slow. Resolution: For this particular issue, PdlRt.exe had a problem with the Page Faults and memory growing. There were so many page faults, that the counter had wrapped around to a negative number, and the memory had grown by around 10 times normal. There have been some fixes in regards to memory usage in Update 7 for WinCC V7.0 SP2. PCS 7 V7.1 SP3 contains WinCC V7.0 SP2 Upd4. To resolve this issue install Update 7 for WinCC V7.0 SP2, or upgrade toPCS 7 V7.1 SP4, whichincludes WinCC V7.0 SP2 Upd8. |
1/23/2013 7:39 AM | |
Joined: 7/3/2010 Last visit: 3/5/2023 Posts: 30 Rating:
|
Dear Woodchuck Try deleting archive files if you don't need it. Regards, Ninad
|
Follow us on