5/13/2012 6:51 PM | |
Posts: 14 Rating: (0) |
Can sm 1234 analogue input module be used as a loop power source to power a two wire sensor like sitrans probe lu. |
5/13/2012 7:51 PM | |
Posts: 14 Rating: (0) |
i used this to connect to the sitrans probe lu and was getting currents of up to 30ma instead of 4-20ma |
5/14/2012 8:29 AM | |
Posts: 272 Rating: (4) |
SM 1234 can be used for the following inputs. 1) +/- 10V 2) 0-20 mA As you have mentioned 4-20 mA kindly ensure the scaling is done for the right count. |
5/14/2012 1:05 PM | |
Joined: 6/26/2009 Last visit: 4/25/2024 Posts: 122 Rating: (23) |
Have a look at this post , it show’s an wiringexample |
5/15/2012 12:33 AM | |
Posts: 14 Rating: (0) |
thanks . will try that |
Follow us on