Industry Online Support
Technical Forum
5/23/2014 8:37 PM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
Hello DavidBrown I am not sure if 25 bit SSI setting on SM 338 will work for a 24 bit SSI encoder. However you can use ET200S SSI Encoder Module : 6ES7 138-4DB03-0AB0 in a ET200S Rack. It supports : 13/14/15/16/17/18/19/20/21/22/23/24/25 Bits !! Here are the Details of : 6ES7 138-4DB03-0AB0 SIMATIC DP, ELECTRONIC MODULE F. ET 200S, 1 SSI 25BIT/1MHZ 15MM WIDE MODULE FOR CONN. OF ABSOLUTE ENCODERS WITH SSI INTERFACE SYNCHRONOUS SERIAL INTERFACE WITH DI AND COMPAR. VALUE WITH CLOCK CYCLIC SYNCHRON. APP Hope this helps Cheers Navnag |
Last edited by: Navnag at: 5/23/2014 8:42 PMThere is no such thing as the last bug in a program |
|
5/27/2014 9:42 PM |
|
Joined: 10/19/2012 Last visit: 4/17/2022 Posts: 315 Rating: (9) |
There is also one available in 1500 series, see below link: |
Follow us on