10/9/2013 9:41 AM | |
Joined: 4/24/2006 Last visit: 2/10/2025 Posts: 8843 Rating:
|
Hello rdoliveira, Please have a look at the following link: What are the functional differences between the different SIMATIC panels? On both panels it is possible to use Sm@rtAccess or Sm@rtService (Or Sm@rtServer) You will have to program in WinCC flexible or WinCC TIA portal project -> Device settings. Best regards, Wizard |
10/9/2013 4:22 PM | |
Joined: 4/24/2006 Last visit: 2/10/2025 Posts: 8843 Rating:
|
Hello rdoliveira, Have you seen this link: Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)? Best regards, Wizard |
This contribution was helpful to
1 thankful Users |
10/10/2013 9:06 AM | |
Joined: 4/24/2006 Last visit: 2/10/2025 Posts: 8843 Rating:
|
Hello rdoliveira, You will need a license on the panel. See also this link: What should you watch out with regard to licenses for WinCC flexible and panels? or What information is available about licenses for WinCC (TIA Portal)? Best regards, Wizard |
Follow us on