10/14/2019 10:55 AM | |
Joined: 11/14/2018 Last visit: 4/3/2025 Posts: 502 Rating:
|
Hello shoaibb95, as a first step to start with, I would suggest this FAQ and the included documentation: It discusses the Sm@rtServer functionality for Industrial Thin Client, but like I said, it may serve as a starting point for you. Greetings, Nzett11 |
If I could help you, be so kind and rate my contribution. :) |
|
10/15/2019 10:21 AM | |
Joined: 6/20/2018 Last visit: 12/18/2024 Posts: 19 Rating:
|
I think I did exactly same but couldn't make it work, on some research found out that I can access HMI over internet through port forwarding, but since I'm a *** in networking so stuck! |
10/21/2019 7:45 AM | |
Joined: 6/20/2018 Last visit: 12/18/2024 Posts: 19 Rating:
|
I've attached a pdf file which contain all the things I did so far, if any one can look into it, it'd be really helpful for me :)
AttachmentRemote Monitoring Over Internet.pdf (209 Downloads) |
10/22/2019 3:11 PM | |
Joined: 8/3/2009 Last visit: 4/17/2025 Posts: 15311 Rating:
|
Helloshoaibb95 There are some Information in this FAQ: https://support.industry.siemens.com/cs/de/en/view/109476153 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on