9/15/2009 8:27 AM | |
Posts: 382 Rating: (47) |
Dear all, I have read the maunal about pin 10 & 11 for SM331. I would like to know something more. Does anyone know what does the symbols for pin 10 & 11 represent for SM331. Is it I.E? [see attach] If both pin 10 & 11 are connected to I.E what will happen? Or not advisable at all? Thanks! with regards, how come? AttachmentSM331 AI block Diagram.pdf (299 Downloads) |
9/15/2009 9:23 AM | |
Joined: 5/28/2008 Last visit: 9/9/2024 Posts: 4515 Rating: (839) |
Dear how come?, As per your attachment, the pins 10 & 11 is used only for compensation.this function is used to make the measurements of analog channelsmore accurite. Here's below the data of the front connector which is suitable with compensation 6ES7392-1AJ20-0AA0 SIMATIC S7-300, FRONT CONNECTOR FOR 6ES7331-7SF00-0AB0, TO IMPROVE THE ACCURANCY OF THERMOCOUPLE MEASUREMENT IN MODE INTERNAL COMPENSATION Please have a look on this FAQ: How can you improve the accuracy of thermocouple measurements? Regards, |
Ayman Elotaify |
|
9/16/2009 8:48 AM | |
Joined: 5/28/2008 Last visit: 9/9/2024 Posts: 4515 Rating: (839) |
Dear how come?, Pin 10 : Comp+ Pin 11: Comp - / Mana. This module is supporting internal and external compensation:
Regards, |
Ayman Elotaify |
|
9/16/2009 5:15 PM | |
Posts: 382 Rating: (47) |
Dear Ayman Elotaify, Thank you much for your explaination. Appreciate! with regards, how come? |
This contribution was helpful to1 thankful Users |
Follow us on