2/7/2019 8:03 AM | |
Posts: 1 Rating:
|
I've been looking at 6ES7511-1CK01-0AB0. What i cant understand is if i have to buy a Communication modul to get communication to out PC? |
2/7/2019 8:59 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
are you the same person who started this thread? S7-1500 PLCs have all an PN-interface. This can be used as Industrial Ethernet interface to communicate over TCP, ISO on TCP or UDP with Open User Communication blocks. But it also depends on your PC and its interfaces, which other communication is maybe also possible. hope this helps, regards, |
FCK WAR! |
|
2/7/2019 10:49 AM | |
Posts: 2826 Rating:
|
( There is an S7-1211 also, which can expand to left {CM} but not expand right {SM}. ) |
2/7/2019 3:06 PM | |
Posts: 5 Rating:
|
Yes its me, was using a collegs login to se the webshop. Thank you very much for you:re answer. |
Follow us on