11/10/2015 10:45 AM | |
Posts: 58 Rating:
|
If you have an operator panel it will display the alarm/fault code. From the operator panel you can acknowledge the fault. Best regards. |
11/10/2015 10:59 AM | |
Joined: 5/12/2006 Last visit: 1/27/2023 Posts: 21197 Rating:
|
no not with a SmartLine without DQ Intefac, here you get no information in teh System! on a SmartLine without DQ you can reset the Fauklt with a Signal on X22.3 (reset), which error exactly occurs is not so easy: X21.2 Prewarning for Temerature Problems DC Link LED for Voltage Level. Refer the Manual for detailed Infromation: https://support.industry.siemens.com/cs/ww/en/view/109479611 Regards Christoph |
This contribution was helpful to
1 thankful Users |
11/10/2015 11:29 AM | |
Joined: 8/19/2014 Last visit: 12/8/2022 Posts: 19 Rating:
|
Thank you very much Chris :) |
Follow us on