Industry Online Support
Technical Forum
8/6/2008 12:23 PM | |
Posts: 5822 Rating: (412)
|
Hello, well there is a sample of a colleague of mine. I hope it works. The Station that sends the SMS is called "Station".# I add the second part of the project in an additional post. Best regards J_Bell AttachmentSms_step1.zip (292 Downloads) |
8/6/2008 12:25 PM | |
Posts: 5822 Rating: (412)
|
Here is the second part of the Archive. Please rename the file from Sms_step1.zip to Sms_step1.z01. Then you can retrieve the files. Best regards J_Bell AttachmentSms_step1.zip (262 Downloads) |
8/11/2008 11:10 AM | |
Posts: 5 Rating: (0) |
Evrything OK. I´ve explained the solution details in the latest Sinaut post. Thanks to everybody |
Follow us on