8/29/2016 12:31 PM | |
Joined: 1/16/2013 Last visit: 6/7/2022 Posts: 47 Rating:
|
I want use Softkey in my diagram, but result is always wrong. On picture 01 is part of diagram. On picture 02 is configuration of Message text. On picture 03 is result. On picture 04 is Resource used of Logo! 8 Why block B325 Softkey is shows as “?N7” ? What does it mean?? Thanks for help Carlos AttachmentSoftkey.zip (35 Downloads) |
Last edited by: carlosovo at: 8/29/2016 12:32:13 PM |
|
8/29/2016 1:24 PM | |
Posts: 2930 Rating:
|
Hi, in your example the Softkey will only do something if you aktivate I3 first. Softwarekey requires a signal HIGH or LOW in front, if you then change the status of the softkey to "ON", then it switches the signal in fromt of it. Check my example to get some experiances. Hope it helps AttachmentSoftkey.zip (39 Downloads) |
This contribution was helpful to
1 thankful Users |
8/29/2016 2:26 PM | |
Joined: 12/18/2014 Last visit: 12/3/2023 Posts: 31538 Rating:
|
In the Logo software problems of various kinds can occur when the block numbers are higher than 200. AttachmentReplace.wmv (39 Downloads) |
This contribution was helpful to
2 thankful Users |
8/30/2016 10:58 AM | |
Posts: 2930 Rating:
|
Hi, the block number was an issue at the beginning of LOGO! 8. I use LOGO! 8 at the beginning and with the todays LOGO! I never had this again. |
Follow us on