4/27/2016 12:31 PM | |
Joined: 6/8/2013 Last visit: 5/15/2024 Posts: 158 Rating: (9) |
Mr. Javed, With the help of Scripting it is possible to communicate with both PLC. |
4/28/2016 10:30 AM | |
Posts: 2 Rating: (0) |
my program i have redudancy plc cpu 315-2dp in mpi and i have CP 343 -1 lean and i connecd it with HMI wincc flexible . i dont know what should i do to make HMI understand the redundancy plc . Attachmentredundancy.pptx (116 Downloads) |
7/16/2016 9:55 PM | |
Joined: 8/16/2015 Last visit: 6/6/2022 Posts: 37 Rating: (0) |
Dear All, Kindly we need your support that i had the configuration of Redundancy for CP343-1 lean with Processor 315-2DP ,i did what exist at Ste_angioni post as the attached image but the communication failed when the Master CP 343-1 failed ,the slave CP not working We didn't know why ? CP A has IP 192.168.0.1 & CP B has IP 192.168.0.2 Saleh AttachmentImage of PLC Comm.zip (118 Downloads) |
7/28/2016 2:10 PM | |
Joined: 8/16/2015 Last visit: 6/6/2022 Posts: 37 Rating: (0) |
Thank you very much Stefano Angioni It's working well now, Regards, Saleh Hany |
Follow us on