1/19/2024 5:43 PM | |
Joined: 4/25/2012 Last visit: 1/13/2025 Posts: 29 Rating: (9) |
I have same issue.. sometimes the values inside a faceplate goes to zero without any reason. The values are write to the plc causing dangerous situations. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/23/2024 11:20:44New subject after splitting |
|
1/19/2024 7:47 PM | |
Joined: 1/21/2013 Last visit: 1/24/2025 Posts: 3462 Rating: (543)
|
Hi, Sorry, but in order to provide helpful feedback, you must provide some meaningful information.
I know this is a long list of questions, but it may not be enough. To get deeper knowledge about your problem, the TIA project would be needed. However, analyzing this sounds like a job for the Siemens support team. So maybe you should contact them by creating a support request. Kind regards |
1/23/2024 7:40 AM | |
Joined: 1/21/2013 Last visit: 1/24/2025 Posts: 3462 Rating: (543)
|
Hi Celio_Goetten, As you said the problem is only related to IO fields, please provide some more features on these IO fields. Is there any event or dynamization being used? If so, please provide details. However, I would strongly recommend you to create a support request. Kind regards |
Follow us on