4/10/2023 9:57 AM | |
Joined: 5/6/2022 Last visit: 9/22/2023 Posts: 289 Rating:
|
Hi SpeedsterJuss, Can I please ask you some more questions about your system set up? Is this PC an IT managed PC, and do you have administrator rights? If you do not have administrator rights for example, you may see this message as Trusted Add-in Catalogs are not allowed. Could you please try it with the Online version of Office Excel, as this should also work. You can also try updating to the latest version of TIA V17; the latest update is update 5. I will link the downloads below. “Updates for STEP 7 V17, S7-PLCSIM V17 and WinCC V17” You may also need the latest version of the Reporting Excel Add-in which you can download with the corresponding WinCC V17 updates. I will also link that below. “Updates for SIMATIC WinCC Unified PC V17” For example, for WinCC V17 Update 5 there should be a download link for the reporting tool under the note: "Download of the Enhancement for the Reporting Excel Addin corresponding to Update 5:" Tell me if this help, if not I will look for another possible solution. Best regards! |
If this Information really helps, you could use the Rate function |
|
Follow us on