11/21/2015 9:59 PM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating: (71) |
Method-1 If you highlight a block in project tree and press "F7" then a windows opens up. Now you have to enter required FB/FC/DB number. After entering press "Enter" and this will open up the required block and will also highlight it under project tree. Method-2 Also relevant FAQ is : How do you sort the blocks in absolute block number order in STEP 7 (TIA Portal)? Opening project overview by keyboard shortcut "Ctrl+2" and then by quickly browsing to required number of FB/FC/DB is faster then trying to find the same block in project tree. Simatic manager rocks while TIA sucks.. |
Last edited by: manmeet at: 11/21/2015 10:09:56 PM |
|
1/4/2017 5:33 PM | |
Posts: 18 Rating: (0) |
Im answering my own question Lol name it yourself as shown in the pic |
This contribution was helpful to1 thankful Users |