5/15/2024 9:18 AM | |
Joined: 1/21/2013 Last visit: 4/18/2025 Posts: 3764 Rating:
|
Hi blyshchak, The two possible solutions I suggested (internal tag or DataSet) can be used in a multi-user environment. DataSet is always for the current session, and an internal tag can be configured to a "local session" scope. To use SetPropertyValue, you must use the object path of the screen object, so 'screen_2' must be available at the moment the method is called. Kind regards |
This contribution was helpful to
1 thankful Users |
Follow us on