5/4/2012 12:48 AM | |
Joined: 6/4/2008 Last visit: 6/2/2024 Posts: 1484 Rating: (322)
|
Hi Rowellrags, Only Siemens personnel have access via Intranet to the resource for spare parts. I have had to make some guesses here, as both your part numbers are wrong. I have deduced that actually, you meant: 1. 6se7034-5uk20 2. 6se7033-0fk20 Again, I have chosen the latest build revision as you did not specify, I have included the image of where to locate the build revision in the zip file. Regards, Graeme
AttachmentDrives.zip (238 Downloads) |
5/4/2012 2:58 PM | |
Joined: 3/13/2012 Last visit: 3/7/2023 Posts: 6 Rating: (0) |
Hi Graeme, In the spare parts list for 6SE7034-5UK20 D which you have provided, I have noticed that the radial ventilator part number is missing. Is it missing or it really doesn't have one? Thanks again. quote user="Graeme"]
Hi Rowellrags, Only Siemens personnel have access via Intranet to the resource for spare parts. I have had to make some guesses here, as both your part numbers are wrong. I have deduced that actually, you meant: 1. 6se7034-5uk20 2. 6se7033-0fk20 Again, I have chosen the latest build revision as you did not specify, I have included the image of where to locate the build revision in the zip file. Regards, Graeme
|
5/4/2012 3:44 PM | |
Joined: 7/8/2009 Last visit: 7/26/2023 Posts: 1974 Rating: (477)
|
Hello, Here is attached spare part list for 6SE7034-5UJ60 6SE7033-0FK60 Regards Devesh AttachmentSpare offer.zip (260 Downloads) |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
5/4/2012 5:01 PM | |
Joined: 3/13/2012 Last visit: 3/7/2023 Posts: 6 Rating: (0) |
Thank you very much Davesh. But just wondering why the radial ventilator (fan) is not among the list of spare parts for 6SE7034-5UK20 D. Do you have any idea why?
|
5/4/2012 6:04 PM | |
Joined: 7/8/2009 Last visit: 7/26/2023 Posts: 1974 Rating: (477)
|
Hello Please find attached spare List for 6SE7034-5UK20 It has FAN in the list Regards, Devesh Vithani Attachment6SE7034-5UK20.zip (211 Downloads) |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
5/4/2012 7:52 PM | |
Joined: 3/13/2012 Last visit: 3/7/2023 Posts: 6 Rating: (0) |
Hi Devesh, Thank you very much. Now, I am confused. I have called the CIC and the Siemens personnel in charge for spare parts had given me a diiferent part number for the fan of this drive 6SE7034-5UK20. A part number which is not in the Siemens mall, and the price is so high. According to him, the part number he gave me is from the factory. In the list that you provided, the operating voltage of the fan is 230 volt AC. But the end user has told me that the operating voltage should be 120 VAC. Unfortunately, the part number given to me from Siemens does not include the desription to tell me the operating voltage of this fan.
|
5/4/2012 11:27 PM | |
Joined: 6/4/2008 Last visit: 6/2/2024 Posts: 1484 Rating: (322)
|
Hi, the voltage for the fans is definately 220VAC The description for the fan module is as follows: 6sy7000-0ab68 - Radial Ventilator 220V 50/60Hz (RH28M-2EK.3F) - Hybrid bearing Voltage: 220V +/- 10% Diameter: 280mm Power: 890W RPM: 2860 Airflow: 2600m3/h Start Cap: 14uF
|
This contribution was helpful to1 thankful Users |
5/7/2012 7:21 PM | |
Joined: 3/13/2012 Last visit: 3/7/2023 Posts: 6 Rating: (0) |
Many thanks Vithani.
|