1/11/2016 1:02 PM | |
Joined: 10/11/2006 Last visit: 10/9/2024 Posts: 5910 Rating: (808)
|
Hello Andreas, I guess that the 24 axes will be coupled mechanically by the line so that the drives share the load, right? If so, the easiest way would be when using G120C to run them in V/Hz control mode and to send all drives the same speed setpoint. This is easy because the load sharing is controlled via the motor slip. The disadvantage of this solution is the low dynamics compared to the servo drive solution. With S120 and its IRT bus you have other option for load sharing applications, like described here: https://support.industry.siemens.com/cs/de/en/view/38470057 When you need to run the axes with angular snychronism, you would need an encoder. |
With best regards, |
|
Follow us on