3/10/2016 9:31 AM | |
Joined: 3/14/2008 Last visit: 9/12/2024 Posts: 2095 Rating: (936) |
Hello Tom, Did you update the PCS7 version? Is your project created in a different version and your trying to migrate? You have to migrate from version to version. You cannot go from v6.1 to 8.0 for example.. Please follow the manual: "Software update with utilization of new functions" depending on your PCS7 current version. |
If I could help you, you can use the RATE button. Thank you. |
|
3/10/2016 2:58 PM | |
Joined: 3/14/2008 Last visit: 9/12/2024 Posts: 2095 Rating: (936) |
Well, When the blocks are updated to the new version, you have to do a full compile of the charts. You can delete the @charts, only if you have F-blocks, which are not updated to the new technology, then they shouldn't be deleted. To which version did you update. I believe you have to update from v6.1 to 7.1 SP3 or SP4. And then to 8.x. Not a update from v6.1 to 7.1 SP1 or SP2.
|
Last edited by: Oreca at: 3/10/2016 3:02:49 PMIf I could help you, you can use the RATE button. Thank you. |
|
3/11/2016 7:12 AM | |
Joined: 3/14/2008 Last visit: 9/12/2024 Posts: 2095 Rating: (936) |
Morning!, Are there any blocks which originate from a PCS7 add-on library, like Simocode or something, which now doesn't work with your new version? |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on