5/20/2014 11:35 AM | |
Joined: 10/3/2010 Last visit: 5/17/2024 Posts: 1552 Rating: (188) |
So client wants 2 monitors on same PC displaying the same WinCC screen? |
B r g d s , |
|
5/21/2014 7:00 AM | |
Joined: 10/3/2010 Last visit: 5/17/2024 Posts: 1552 Rating: (188) |
Hey YogendraG, If both monitors always display the same WinCC picture, you can just do it by using the Multiple monitor setting of your windows, here you can choose between extended desktop or duplicate desktop. Last option means both monitors of your PC always show exactly the same screen. If both monitors should be able to navigate in WinCC independantly, you'll have to do some work all over again, starting with your start screen. You can try to create a new start screen with the geometry of both monitors together, inside you have 2 picture windows, each with the screen size of one monitor. Inside each of those 2 picture windows, you call the original start screen (chance of success depends on how your project and navigation is made). Under Computer Propertiesn select tab Graphics Runtime and select "Hide main window" (Independent Picture Window). |
B r g d s , |
|
5/21/2014 1:15 PM | |
Joined: 10/3/2010 Last visit: 5/17/2024 Posts: 1552 Rating: (188) |
So Windows duplicating desktop is the only good choice. |
B r g d s , |
|
Follow us on