9/17/2024 7:07 AM | |
Joined: 5/6/2022 Last visit: 10/4/2024 Posts: 461 Rating: (90) |
The first thing I would like to ask you is which version of TIA Portal Unified are you working with and which image version do you have in the panel? On the other hand, in principle this should be possible by means of the following scritpt: "Driver={SQLite3};Database=/media/simatic/X51/MyUCP.db;trusted_connection=yes;"; Check that in the one you have developed you have not forgotten any ";" and make sure there are no spaces in the string. Additionally I share with you a link that may be useful: "SIMATIC HMI WinCC Unified V19: Connecting Unified Comfort Panel with SQL database" I hope it can help. Best regards! |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
10/2/2024 2:27 PM | |
Joined: 1/16/2019 Last visit: 10/2/2024 Posts: 1 Rating: (0) |
Hello you have a fix?? i have the same problem on the TP1500 Unified |
Follow us on