8/24/2013 2:45 AM | |
Posts: 3 Rating:
|
Hello, I have installed the scout v4.3.1.12, but SSP CU250S VECTOR can't install . Pls tell me correct link. Thanks Bob AttachmentInstall_SSP_SINAMICS_G120_CU250S_VECTOR_V4_6__04.60.10.03_Log.zip (454 Downloads) |
8/24/2013 7:24 PM | |
Joined: 5/12/2006 Last visit: 4/23/2025 Posts: 22623 Rating:
|
Hello, there is no SSP CU250 available for SIMOTION Scout at the moment. Regards Christoph |
8/26/2013 9:03 AM | |
Posts: 116 Rating:
|
Hi, see http://support.automation.siemens.com/WW/view/en/77498613 4. Prerequisites / dependencies Start of delivery of the CU250S-2 vector is scheduled with the SINAMICS Pool Firmware V4.6 HF4. The Control Unit can be configured with the STARTER Version V4.3 SP2 (or later). |
Follow us on