12/7/2021 5:40 PM | |
Joined: 2/17/2020 Last visit: 3/20/2025 Posts: 1236 Rating:
|
Hi Ricor5, Please try the following : - Check the IIS services, if all are activated. Which Windows functions must be activated in order to be able to install SIMATIC WinCC Unified? - Check if "SIMATIC WinCC Unified PC Simulation" is installed on the computer. - Restart the computer and test the behavior with a new project. If the behavior occurs again after activating the missing services, I would suggest : - Uninstall WinCC Unified |
A rating will be well appreciated. |
|
This contribution was helpful to
3 thankful Users |
Follow us on