1/29/2016 11:26 AM | |
Posts: 31 Rating:
|
hello, I am working on pedal robot which i need to run with power module 340 (sinamics s120) with CU305 Dp. in order to run with starter I downloaded the program starter V4.4 for G110 and 120( because I could not able to find starter program for S120) first of all : should I find starter program exactly for S120? if yes, where is the link for this program. if it is ok to work also with sinamics S120, during running PG/PC it gives me the notification which says: it can not find accessible nodes and so it gives me the error for connection. I connect with RS232 with pc and I chose serial port in the configuration. I am waiting for kind response from this frum. please help me ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 1/31/2016 2:46:54 PMNew subject after splitting |
|
1/29/2016 12:07 PM | |
Joined: 5/12/2006 Last visit: 7/25/2024 Posts: 22324 Rating:
|
Hello, there is no starter specific to a SINAMICS Drive Family, the Starter support all SINAMCIS Drives. Which interface you have connected from the S110 CU305DP to the PC? Download all Volumes of Starter from her: https://support.industry.siemens.com/cs/ww/en/view/26233208 Then extract the dowloaded volumes exaclty like described and install the starter with all SSP, then the S110 CU305DP should also installed. Which FW Version do you have for the S110 CU305DP?
Christoph |
Last edited by: ChristophD at: 1/29/2016 12:10:20 PM |
|
2/1/2016 1:12 PM | |
Joined: 5/12/2006 Last visit: 7/25/2024 Posts: 22324 Rating:
|
Hello, right PPI is the RS232 interface. Do you have a COM Port in the PC or a USB2COM Adapter used? Regards Christoph |
2/1/2016 1:19 PM | |
Posts: 31 Rating:
|
Hello, I have com port. |
Follow us on