6/2/2014 8:08 AM | |
Joined: 9/23/2013 Last visit: 10/11/2024 Posts: 47 Rating: (0) |
On S120 cu320 And G120 Cu240e-2 dp-f |
6/3/2014 7:12 AM | |
Posts: 57 Rating: (0) |
Hi, All the control units of sinamics G-120 does not support trace function. Hence the limitation lies in the hardware (CU) and not in the software (starter).
|
6/3/2014 1:08 PM | |
Joined: 10/11/2006 Last visit: 10/11/2024 Posts: 5911 Rating: (809)
|
have you installed Hotfix 1 already: |
With best regards, |
|
6/5/2014 3:58 PM | |
Joined: 10/11/2006 Last visit: 10/11/2024 Posts: 5911 Rating: (809)
|
Hello, In the Hotfix 1 for the STARTER V4.3 SP3, the following restrictions has been corrected:
Hotfix 1 for SINAMICS MICROMASTER STARTER V4.3 SP3. |
With best regards, |
|
Follow us on