Industry Online Support
Technical Forum
8/6/2011 8:14 AM | |
Posts: 1 Rating: (0) |
We have a Step5 PLC for controlling our refrigerants compressor. Mentioned PLC included two racks, one for redundant CPUs and the other for I/Os. The exact configuration of racks is attached to this thread. For monitoring of compressor WinCC program is used by means a CP that was installed in extension rack. Leili EsmaeilaniDuring following days multiple trips occurred and in each of them at least one of the CPUs went to Stop mode with needs to Cold restart. It may be useful to mention in all these cases stop led on CPU was blinking and BASP led was lit except for the last trip that in one of the CPUs the ZYK Led was lit too. In each of the stop conditions we gather the information of IStack & BStack of stopped PLC that have been attached to this thread. In addition to above investigations, we have changed some of hardware to rectify the error without any exact reason and only some guesses, for example we have changed the extension rack Power Supply, as we had an experience of failing of it in another similar package. Also we have changed the Power Supply modules in CPU racks, one of the CPUs and two communication modules that connect the CPUs together for redundancy. Although all mentioned activities the problem has not rectified and we have no idea to start with. Would you please investigate the situation and help us with your respectful advices. AttachmentStep5.zip (216 Downloads) |
Last edited by: CS Moderator at: 8/7/2011 11:03 PMContact data deleted |
|
8/18/2011 2:56 PM | |
Joined: 6/22/2009 Last visit: 5/24/2024 Posts: 62 Rating: (3) |
Hello, Your hardware config shows CPU948R. Your ISTACK shows stop at OB110, OB111. Did you change CPU928 to CPU948 and kept the same program? Please download manual of 948 from the link below and refer to section 1-21. The program seems wrong. Regards https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&siteid=cseus&aktprim=0&extranet=standard&viewreg=WW&objid=10805082&treeLang=en |
Follow us on