7/11/2011 10:05 AM | |
Posts: 270 Rating: (53) |
Hello Anton, the problem is in incompatibility of Win XP SP3 with Step5 V7.23, see following link for details and also a tip on the SP3 uninstallation. Next time I also suggest use search before posting your problem, you will get your answer faster. /tf/WW/en/Posts/25963 |
7/11/2011 10:37 AM | |
Posts: 376 Rating: (57) |
Hello Anton, I think also. The cause for the problem can be the configuration Win XP+SP3 and STEP 5 V7.23. STEP 5 V7.23 is only released for Windows XP Professional + SP1 and Windows XP Professional + SP2. So please uninstall SP3 and try again with installation of Step 5. Another cause is not currently known to me.My recommendation for you. If you need. The Hotfix 1 for STEP 5 V7.23 is available. Here the Link: http://support.automation.siemens.com/WW/view/en/19348145Best Regards Gucci |
7/11/2011 11:40 AM | |
Posts: 270 Rating: (53) |
Well that's tough luck, but not surprising, old installers weren't really all that sophisticated. I found one match on google regarding your topic, however, it's in Chinese and our awesome supersmart proxy doesn't let me use the translate page link, so perhaps if it would work for you, maybe you could find something useful there. |
Last edited by: MM1234 at: 7/11/2011 11:41 AMP.S. your english is fine, it was me missunderstanding before, need more coffee I guess .] |
|
Follow us on