5/23/2018 8:12 PM | |
Posts: 1 Rating:
|
Good day sir. I Have field pg M3 with step 5 V7.23 + S5 prog adapter. When configured type prommer: internal the system shou error message that said: drive error ! Programable controller has a hardware conflict with another device. You have already used a device on the same adress of programmable controller. Current driver: S5MCD.SYS Error: 0x0000 Driver function: 0x09 Error: 0x0478 Can you help me please. What can be happing? Thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 5/24/2018 6:41:43 AMNew subject after splitting |
|
5/25/2018 2:12 AM | |
Joined: 9/28/2010 Last visit: 5/4/2022 Posts: 5 Rating:
|
Hello friends: I have the same problem and my screen show this message. |
5/28/2018 6:13 PM | |
Posts: 2 Rating:
|
Hello, friends. The problem has been resolved. The software was reinstalled, some programs In the field pg M3 that used the same port were blocked, and the EPROM memory was replaced. Thank you for my own help! See you partners...
|
This contribution was helpful to
1 thankful Users |
Follow us on