10/7/2010 12:33 PM | |
Posts: 8 Rating: (0) |
Hi, I am facing a problem with installing Step 7 Basic v 10.5 software. I will briefly explain what happened so that you can get a clearer view of the error. Initially I installed Step 7 Basic v 10.5 without any errors. I also started programming the CPU 1212C PLC. After a couple of days, the software stopped working. The error was that whenever I opened the software it said "The Application has encountered a problem and needs to close. Would you like to restart the application?" (Attached image 1.jpg)The options given were Restart and Close. When I chose to press Restart, it would show the same error message again. When I pressed Close and then tried to start the application, it would give me the same error. I thought something must have gone wrong with a few files. So I decided to uninstall the application completely and reinstall it again. When I tried to reinstall, there was an error message which said - "An error occurred during setup" (Attached image 2.jpg) and the only thing I could do was close the setup. After that I went into the registry of my computer and deleted folders in LocalMachine/Siemens/Automation/TIAv10.5 (I don't remember the exact name but it was only of Step7 Basic.) I tried to reinstall the software after that. But I got the same error as I had previously encountered.I am attaching the Log File which was created during the Installation, Please let me know what to do. Thanks in advance for the help. P.S. I have put 1.jpg, 2.jpg and the Error Log text file in the attached Errors.zip file AttachmentErrors.zip (626 Downloads) |
10/7/2010 3:06 PM | |
Joined: 6/29/2010 Last visit: 10/27/2022 Posts: 112 Rating: (63) |
Hi Vinay L, I saw in your log file that yours operation system is a "Microsoft Windows NT 5.1.2600 Service Pack 3", the TIA Portal 10.5 cannot to be instaled at this operation system, the requirements to install the TIA Portal 10.5 are http://support.automation.siemens.com/BR/view/en/42100716. Regards. |
10/7/2010 4:16 PM | |
Joined: 11/15/2006 Last visit: 5/7/2021 Posts: 1319 Rating: (170) |
Do a uninstall of all .Net Frameworks and reinstall them. Could be a kind of .Net problem. |
Have Fun! |
|
10/8/2010 4:09 AM | |
Posts: 8 Rating: (0) |
Strange. I am not quite sure how the Operating System was recognized as Windows NT . Because I have a Windows XP operating system with Service Pack 3. Attaching a screenshot. @TomDeWou - Thanks for the suggestion. I will keep this in mind. Iwilldo that as a last resort as the .NET framework is being utilized by a lot of other softwares. As was said earlier, the software was running fine for a couple of days. The only thing that changed was maybe a Siemens IT HelpDesk runsecurity update on our systems. |
10/13/2010 7:37 AM | |
Posts: 8 Rating: (0) |
This problem is yet to be solved. Please do let me know if you have the solution for this. :) |
Follow us on