9/3/2006 3:46 PM | |
Joined: 1/7/2006 Last visit: 2/16/2023 Posts: 2705 Rating:
|
Hi Jack, Maybe you can make a ASCII-file from the data and put that in a editor to change and get it back in to the editor. You may make a ASCII source by doing the next, open the editor by doubleclicking on a DB that you want to convert to a source. Then go to the menupoint "File" --> "Generate Source...", chose a objectname and "ok", now you may chose which blocks you want to convert. Give in the blocks and after that you have a ASCII-file that can be exportet to Excel. See the document to get some more information. AttachmentWork with Sources.pdf (368 Downloads) |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on